Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
pwr diss
Another consideration is the power dissipation of the SSR in its operating environment. For example, the PS7141E-1A has an allowed maximum power dissipation of 560 mW. The power dissipation of each device in the circuit can contribute to the overall ambient temperature of the operating equipment. Calculation of the Power Dissipation is as follows: The total power consumption (PT) of the PS7141-1A is the sum of power consumption (PE) of the IRED on the input side (primary side) and power consumption (Po) of the light receiving PVD and IC on the output side (MOSFET side), or PT = PE + PO.
PTM Veröffentlicht am: