Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 11

It is possible to compensate for the torque ripple by increasing the current in the one winding that is turned on during the half step so that the magnitude of the magnetic vector is the same as it would be if both of the windings were energized. If the current is increased in the one ON coil by a factor of the square root of 2, then the same magnitude of vector will be produced when only one coil is ON as is produced when the two coils are driven by the same current. The current waveforms shown here have been modified to use this technique to control the current and reduce the torque ripple. This can easily be done with some of the control IC’s by simply changing a reference for the motor current.

PTM Veröffentlicht am: