Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 18

When this point is reached, the motor has most likely already stalled if it has any load on it. Since the torque is proportional to the current in the motor, the torque will decrease as the peak current decreases. An earlier slide showed the speed torque curve with a downward slope at increasing speed. This reduction in the peak current at higher speed is one of the contributing factors. If the time constant of the current could be decreased, better performance from the motor can be expected.

PTM Veröffentlicht am: