Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 28

This graph shows the actual operating waveforms implemented with an L6208 for a microstepping drive. Channels 2 and 3, the green and purple traces, are the output of the DAC for the two coils. Channel 4, the magenta trace, shows the current in the winding corresponding to the reference voltage on channel 2. Channel 1 shows the step clock input that controls the phase relationship of the bridge. In this example the sine wave is synthesized using 16 microsteps per step, dividing each 90° into sixteen 5.63° microsteps. This implementation uses an 8 bit DAC, actually a RC filter on a PWM output from a microcontroller, to generate the two reference voltages. As a rule of thumb, two additional bits are needed in the DAC above the number of microsteps to generate an acceptable sine wave. For the 16 microsteps shown here, a 6 bit DAC would be sufficient. With an 8 Bit DAC, an acceptable approximation can be created for the two sine waves for a 64 microstep application. Typically 1/16 to 1/32 microstepping can be achieved with most motors. How well the motor will follow the microsteppping waveform depends on its construction.

PTM Veröffentlicht am: