Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 4

There are two common configurations for stepper motors, the two phase bipolar motor and the four phase unipolar motor. In their simplest form, as shown in the figure, there is a permanent magnet on the rotor and two coils oriented at 90° to each other on the stator. When driven, the current in each of the coils produce magnetic vectors that sum together with the permanent magnet on the rotor aligning with this combined magnetic vector. Changing the polarity of the current will change the angle of the magnetic vector and thus generate the rotating magnetic field that will make the motor turn. For the bipolar motor, this is done by sequentially changing the polarity of the current in the two windings. For the unipolar motor, the coil is wound in a center tapped configuration with the center typically connected to a positive supply voltage. Alternately connecting the two end connections to ground will change the direction of the resulting magnetic vector.

PTM Veröffentlicht am: