Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 36

Looking at microstepping applications, achieving zero current by simply applying a zero reference is not possible. The value of the minimum current may also affect how well the circuit can match the sine wave it is trying to synthesize. This graph shows the ideal waveforms for a micostepping drive running at a constant speed. The phase relationship between the two signals determines the direction of rotation.

PTM Veröffentlicht am: