Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 25

Up to this point in the presentation only full step or half step operation has been discussed. These motors are limited to 4 or 8 positions per electrical cycle, and are naturally achieved by controlling the phase relationship of the currents without changing the magnitude. For applications that require higher resolution in positioning, it is possible to drive a stepper motor to positions between the full and half step positions. This is generally referred to as microstepping.

PTM Veröffentlicht am: