Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 22

Using the chopper controlled current drive to drive the stepper motor provides a very fast current rise and good efficiency in the circuit. Comparing the current waveform to the previous example, there is a slight improvement in the rise time compared to the L over nR configuration. This example shows the same motor from earlier operating at 5 times the rated voltage (25V) with a chopper current control set to control a peak current of 1A. There are a lot of advantages to using the chopper drive that improve the performance and give a very good efficiency. The disadvantages of complexity and additional circuitry have mostly been overcome by integrated motor drivers that include all of the control circuitry and, in many cases, also the power transistors on a single monolithic IC. Although some low end applications are still designed using a simple L over R drive and a unipolar motor, most applications today use a chopper drive with integrated driver ICs to drive bipolar stepper motors.

PTM Veröffentlicht am: