Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 13

A typical 5V, 1A stepper motor will have a 5Ω resistance. When the coil is energized, the current increases exponentially until it reaches its full value of 1A. As shown in the figure, this can be relatively slow. To drive the motor faster, the time for each step decreases. As the step time becomes shorter and shorter, it will reach a point where the step time is nearly the same as the time constant for the coil.

PTM Veröffentlicht am: