Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 24

This figure shows a comparison between fast and slow decay modes of operation. Two things are important to notice. First, the ripple current is much higher in the fast decay mode. Second, the current decays or decreases much faster in the fast decay mode. For most applications that are operated in full step or half step sequences, the slow decay mode is probably a better choice since it gives less ripple in the current. Many times it will also have less dissipation in the driver, but this is not always the case. The fast decay has an advantage if the current must decay rapidly, which is required in some applications.

PTM Veröffentlicht am: