Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 31

During operation, the motor current is compared to a reference, Iref. In the circuit implementation, the current is represented by the voltage across the sense resistor and the reference is really the Vref applied to the comparator. It is expected that as the reference is reduced, the duty cycle will decrease and the current will also decrease proportionally. Ideally following a linear transfer curve like the dashed blue line.

PTM Veröffentlicht am: