Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 12

The simplest topology is to drive the motor with the rated voltage and simply switch the coils in sequence, as shown in the full step or half step sequences. The figure here represents such a drive topology. The circuit has been simplified with the single transistor representing one of transistors of a unipolar drive or the composite of two transistors in the bridge of a bipolar drive. When the phase is energized the current will increase exponentially until it reaches a value that is equal to the supply voltage divided by the motor resistance, Rc. The time constant of the exponential is L divided by R which gives rise to the name L over R drive. This drive configuration is very simple, requires no additional components beyond those required to control the current sequence and operates from a single supply voltage. However, it exhibits relatively low performance in terms of the speed torque profile. One of the reasons the performance is limited is due to the inductive properties of the coils that limit the rate of change of current.

PTM Veröffentlicht am: