Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 3

Stepper motors are well suited for low torque applications that need precise position control, such as computer peripherals or numerically controlled machine tools. In these applications, steppers have several advantages. Since they have no brushes, they are highly reliable motors whose life is essentially determined by the life of the bearings or bushings in the motor. The control loop is very cheap since the motor is driven open loop without any position or speed feedback elements. Since the motor is a synchronous machine, speed control is simple. The motor configuration inherently provides good position control.

PTM Veröffentlicht am: