Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 46

For most applications, this can be done with a simple linear ramp for acceleration and deceleration. The starting speed is set by the blue line in the previous slide, and the maximum is set by the green line. The blue line in the slide shows a typical move speed profile. For each movement, the step time is gradually reduced for each step, starting from the time set to overcome the inertia of the load, until the desired speed is achieved. The procedure is reversed to decelerate the motor, gradually increasing the step time each step. For short moves the motor may not reach the full speed before it needs to start decelerating, so the acceleration may have to be truncated as shown by the green line. The discontinuities at the corners of this acceleration profile correspond to a change in the acceleration or jerk. In some applications, like moving fluid, it may be necessary to reduce the jerk. This can be accomplished by rounding the corners at the top of the movement profile.

PTM Veröffentlicht am: