Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 39

Another anomaly that can affect microstepping is a result of the decay mode that is selected. These two different decay modes, fast decay and slow decay, were discussed earlier. In the slow decay mode, during the off time, the current is re-circulating around a path that is one on transistor and one diode (or one MOS conducting in the reverse direction). During this time, the current decays rather slowly since the voltage across the coil is very small. However, the slow decay rate may limit the ability to follow a fast changing waveform that is on the downward slope of the sine curve. The green and orange traces represent the current waveform when the decay rate is limited by the slow decay and the inductance of the motor. Since the entire voltage is applied across the motor when energizing the inductance, the di/dt can be relatively fast. In that case the current can follow the rising slope of the sine wave but the fall time is limited by di/dt.

PTM Veröffentlicht am: