Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 43

For a stepper motor drive, the designer must consider the speed-torque performance of the motor and guarantee that it is always operating under the speed-torque curve of the motor. If the available torque at a given speed is exceeded, the motor will stall and stop. This figure shows a typical speed-torque curve for a stepper motor. Notice the downward slope at higher speeds. Although this curve can be found on the motor’s datasheet, the real performance curve has some discontinuities.

PTM Veröffentlicht am: